SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
There are three subscribers in the AON event fabric as can be seen in Figure 6-4. The first subscriber is the MCU event fabric, which resides in the MCU power domain. The other two subscribers, the WUC and RTC, both reside in the AON power domain and are presented in the following subsections.