SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
Each channel implements 15 different channel actions. They are categorized as one-shot and continuous:
Table 20-30 lists the 15 channel actions.
| Index | Channel Action | Category |
|---|---|---|
| 0 | Disable channel | One-shot |
| 1 | Set on capture, and then disable channel | One-shot |
| 2 | Clear on zero, toggle on compare, and then disable channel | One-shot |
| 3 | Set on zero, toggle on compare, and then disable channel | One-shot |
| 4 | Clear on compare, and then disable channel | One-shot |
| 5 | Set on compare, and then disable channel | One-shot |
| 6 | Toggle on compare, and then disable channel | One-shot |
| 7 | Pulse on compare, and then disable channel | One-shot |
| 8 | Period and pulse width measurement | Continuous |
| 9 | Set on capture repeatedly | Continuous |
| 10 | Clear on zero, toggle on compare repeatedly | Continuous |
| 11 | Set on zero, toggle on compare repeatedly | Continuous |
| 12 | Clear on compare repeatedly | Continuous |
| 13 | Set on compare repeatedly | Continuous |
| 14 | Toggle on compare repeatedly | Continuous |
| 15 | Pulse on compare repeatedly | Continuous |
After configuration, the channel requests updates of enabled event outputs according to the channel action description in Table 20-30. There are three channel actions that require further description.