SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
Command ID number: 0x0006
CMD_REMOVE_DATA_ENTRY is an immediate command that takes the parameters listed in
Table 26-54.
| Byte Index | Field Name | Bits | Bit Field Name | Type | Description |
|---|---|---|---|---|---|
| 0–1 | commandNo | W | The command ID number | ||
| 2–3 | Reserved | ||||
| 4–7 | pQueue | W | Pointer to the queue structure from which the entry is removed | ||
| 8–11 | pEntry | R | Pointer to the entry that was removed |
On reception, the radio CPU removes the first data entry from the queue indicated. The command returns a pointer to the entry that was removed. The radio CPU performs the following operations:
Set pEntry = pQueue->pCurrEntry
Set pQueue->pCurrEntry = pEntry->pNextEntry
Set pEntry->status = Finished
If the pointer pQueue is invalid, the command fails, and the radio CPU sets the result byte of CMDSTA to ParError. If the queue specified in pQueue is empty, the command fails, and the radio CPU sets the result byte of CMDSTA to QueueError. If the entry to be removed is in the BUSY state, the command fails, and the radio CPU sets the result byte of CMDSTA to QueueBusy.