SWCU192 November 2021 CC1312R7 , CC1352P7 , CC2652P7 , CC2652R7
#AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_TABLE_1 lists the memory-mapped registers for the AUX_SYSIF registers. All register offset addresses not listed in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_TABLE_1 should be considered as reserved locations and the register contents should not be modified.
Complex bit access types are encoded to fit into small table cells. #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_LEGEND shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| RH | R H | Read Set or cleared by hardware |
| Write Type | ||
| W | W | Write |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
OPMODEREQ is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_OPMODEREQ_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_OPMODEREQ_TABLE.
Return to the Summary Table.
Operational Mode Request
AUX can operate in three operational modes. Each mode is associated with:
- a SCE clock source or rate, given by AON_PMCTL:AUXSCECLK. This rate is termed SCE_RATE.
- a system power supply state request. AUX can request powerdown (uLDO) or active (GLDO or DCDC) system power supply state.
- a specific system response to an active AUX wakeup flag. The response is dependent on what operational mode is requested.
uLDO power supply state offers limited current supply. AUX_SCE cannot use certain peripherals and functions such as AUX_DDI0_OSC, AUX_TDC and AUX_ANAIF ADC interface in this power supply state.
Follow these rules:
- It is not allowed to change a request until it has been acknowledged through OPMODEACK.
- A change in mode request must happen stepwise along this sequence, the direction is irrelevant:
PDA - A - LP - PDLP.
Failure to follow these rules might result in unexpected behavior and must be avoided.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | REQ | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1-0 | REQ | R/W | 0h | AUX operational mode request.
0h = Active operational mode, characterized by: 1h = Lowpower operational mode, characterized by: 2h = Powerdown operational mode with wakeup to active mode, characterized by: 3h = Powerdown operational mode with wakeup to lowpower mode, characterized by: |
OPMODEACK is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_OPMODEACK_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_OPMODEACK_TABLE.
Return to the Summary Table.
Operational Mode Acknowledgement
AUX_SCE program must assume that the current operational mode is the one acknowledged.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ACK | ||||||||||||||
| R-0h | R-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1-0 | ACK | R | 0h | AUX operational mode acknowledgement.
0h = Active operational mode is acknowledged. 1h = Lowpower operational mode is acknowledged. 2h = Powerdown operational mode with wakeup to active mode is acknowledged. 3h = Powerdown operational mode with wakeup to lowpower mode is acknowledged. |
PROGWU0CFG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU0CFG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU0CFG_TABLE.
Return to the Summary Table.
Programmable Wakeup 0 Configuration
Configure this register to enable a customized AUX wakeup flag. The wakeup flag will be captured by AON_PMCTL which responds according to the current operational mode. You can select WUFLAGS.PROG_WU0 to trigger execution of a programmable AUX_SCE vector by configuration of VECCFGn. You need to follow the procedure described in WUFLAGSCLR to clear this flag. You need to follow the procedure described in WUGATE to configure it.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | POL | EN | WU_SRC | ||||||||||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | POL | R/W | 0h | Polarity of WU_SRC. The procedure used to clear the wakeup flag decides level or edge sensitivity, see WUFLAGSCLR.PROG_WU0. 0h = The wakeup flag is set when WU_SRC is high or goes high. 1h = The wakeup flag is set when WU_SRC is low or goes low. |
| 6 | EN | R/W | 0h | Programmable wakeup flag enable. 0: Disable wakeup flag. 1: Enable wakeup flag. |
| 5-0 | WU_SRC | R/W | 0h | Wakeup source from the asynchronous AUX event bus. Only change WU_SRC when EN is 0 or WUFLAGSCLR.PROG_WU0 is 1. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
PROGWU1CFG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU1CFG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU1CFG_TABLE.
Return to the Summary Table.
Programmable Wakeup 1 Configuration
Configure this register to enable a customized AUX wakeup flag. The wakeup flag will be captured by AON_PMCTL which responds according to the current operational mode. You can select WUFLAGS.PROG_WU1 to trigger execution of a programmable AUX_SCE vector by configuration of VECCFGn. You need to follow the procedure described in WUFLAGSCLR to clear this flag. You need to follow the procedure described in WUGATE to configure it.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | POL | EN | WU_SRC | ||||||||||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | POL | R/W | 0h | Polarity of WU_SRC. The procedure used to clear the wakeup flag decides level or edge sensitivity, see WUFLAGSCLR.PROG_WU1. 0h = The wakeup flag is set when WU_SRC is high or goes high. 1h = The wakeup flag is set when WU_SRC is low or goes low. |
| 6 | EN | R/W | 0h | Programmable wakeup flag enable. 0: Disable wakeup flag. 1: Enable wakeup flag. |
| 5-0 | WU_SRC | R/W | 0h | Wakeup source from the asynchronous AUX event bus. Only change WU_SRC when EN is 0 or WUFLAGSCLR.PROG_WU1 is 1. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
PROGWU2CFG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU2CFG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU2CFG_TABLE.
Return to the Summary Table.
Programmable Wakeup 2 Configuration
Configure this register to enable a customized AUX wakeup flag. The wakeup flag will be captured by AON_PMCTL which responds according to the current operational mode. You can select WUFLAGS.PROG_WU2 to trigger execution of a programmable AUX_SCE vector by configuration of VECCFGn. You need to follow the procedure described in WUFLAGSCLR to clear this flag. You need to follow the procedure described in WUGATE to configure it.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | POL | EN | WU_SRC | ||||||||||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | POL | R/W | 0h | Polarity of WU_SRC. The procedure used to clear the wakeup flag decides level or edge sensitivity, see WUFLAGSCLR.PROG_WU2. 0h = The wakeup flag is set when WU_SRC is high or goes high. 1h = The wakeup flag is set when WU_SRC is low or goes low. |
| 6 | EN | R/W | 0h | Programmable wakeup flag enable. 0: Disable wakeup flag. 1: Enable wakeup flag. |
| 5-0 | WU_SRC | R/W | 0h | Wakeup source from the asynchronous AUX event bus. Only change WU_SRC when EN is 0 or WUFLAGSCLR.PROG_WU2 is 1. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
PROGWU3CFG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU3CFG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PROGWU3CFG_TABLE.
Return to the Summary Table.
Programmable Wakeup 3 Configuration
Configure this register to enable a customized AUX wakeup flag. The wakeup flag will be captured by AON_PMCTL which responds according to the current operational mode. You can select WUFLAGS.PROG_WU3 to trigger execution of a programmable AUX_SCE vector by configuration of VECCFGn. You need to follow the procedure described in WUFLAGSCLR to clear this flag. You need to follow the procedure described in WUGATE to configure it.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | POL | EN | WU_SRC | ||||||||||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | POL | R/W | 0h | Polarity of WU_SRC. The procedure used to clear the wakeup flag decides level or edge sensitivity, see WUFLAGSCLR.PROG_WU3. 0h = The wakeup flag is set when WU_SRC is high or goes high. 1h = The wakeup flag is set when WU_SRC is low or goes low. |
| 6 | EN | R/W | 0h | Programmable wakeup flag enable. 0: Disable wakeup flag. 1: Enable wakeup flag. |
| 5-0 | WU_SRC | R/W | 0h | Wakeup source from the asynchronous AUX event bus. Only change WU_SRC when EN is 0 or WUFLAGSCLR.PROG_WU3 is 1. If you write a non-enumerated value the behavior is identical to NO_EVENT. The written value is returned when read. 0h = AUX_EVCTL:EVSTAT0.AUXIO0 1h = AUX_EVCTL:EVSTAT0.AUXIO1 2h = AUX_EVCTL:EVSTAT0.AUXIO2 3h = AUX_EVCTL:EVSTAT0.AUXIO3 4h = AUX_EVCTL:EVSTAT0.AUXIO4 5h = AUX_EVCTL:EVSTAT0.AUXIO5 6h = AUX_EVCTL:EVSTAT0.AUXIO6 7h = AUX_EVCTL:EVSTAT0.AUXIO7 8h = AUX_EVCTL:EVSTAT0.AUXIO8 9h = AUX_EVCTL:EVSTAT0.AUXIO9 Ah = AUX_EVCTL:EVSTAT0.AUXIO10 Bh = AUX_EVCTL:EVSTAT0.AUXIO11 Ch = AUX_EVCTL:EVSTAT0.AUXIO12 Dh = AUX_EVCTL:EVSTAT0.AUXIO13 Eh = AUX_EVCTL:EVSTAT0.AUXIO14 Fh = AUX_EVCTL:EVSTAT0.AUXIO15 10h = AUX_EVCTL:EVSTAT1.AUXIO16 11h = AUX_EVCTL:EVSTAT1.AUXIO17 12h = AUX_EVCTL:EVSTAT1.AUXIO18 13h = AUX_EVCTL:EVSTAT1.AUXIO19 14h = AUX_EVCTL:EVSTAT1.AUXIO20 15h = AUX_EVCTL:EVSTAT1.AUXIO21 16h = AUX_EVCTL:EVSTAT1.AUXIO22 17h = AUX_EVCTL:EVSTAT1.AUXIO23 18h = AUX_EVCTL:EVSTAT1.AUXIO24 19h = AUX_EVCTL:EVSTAT1.AUXIO25 1Ah = AUX_EVCTL:EVSTAT1.AUXIO26 1Bh = AUX_EVCTL:EVSTAT1.AUXIO27 1Ch = AUX_EVCTL:EVSTAT1.AUXIO28 1Dh = AUX_EVCTL:EVSTAT1.AUXIO29 1Eh = AUX_EVCTL:EVSTAT1.AUXIO30 1Fh = AUX_EVCTL:EVSTAT1.AUXIO31 20h = AUX_EVCTL:EVSTAT2.MANUAL_EV 21h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2 22h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY 23h = AUX_EVCTL:EVSTAT2.AON_RTC_4KHZ 24h = AUX_EVCTL:EVSTAT2.AON_BATMON_BAT_UPD 25h = AUX_EVCTL:EVSTAT2.AON_BATMON_TEMP_UPD 26h = AUX_EVCTL:EVSTAT2.SCLK_LF 27h = AUX_EVCTL:EVSTAT2.PWR_DWN 28h = AUX_EVCTL:EVSTAT2.MCU_ACTIVE 29h = AUX_EVCTL:EVSTAT2.VDDR_RECHARGE 2Ah = AUX_EVCTL:EVSTAT2.ACLK_REF 2Bh = AUX_EVCTL:EVSTAT2.MCU_EV 2Ch = AUX_EVCTL:EVSTAT2.MCU_OBSMUX0 2Dh = AUX_EVCTL:EVSTAT2.MCU_OBSMUX1 2Eh = AUX_EVCTL:EVSTAT2.AUX_COMPA 2Fh = AUX_EVCTL:EVSTAT2.AUX_COMPB 30h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 31h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 32h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 33h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 34h = AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 35h = AUX_EVCTL:EVSTAT3.AUX_TIMER1_EV 36h = AUX_EVCTL:EVSTAT3.AUX_TIMER0_EV 37h = AUX_EVCTL:EVSTAT3.AUX_TDC_DONE 38h = AUX_EVCTL:EVSTAT3.AUX_ISRC_RESET_N 39h = AUX_EVCTL:EVSTAT3.AUX_ADC_DONE 3Ah = AUX_EVCTL:EVSTAT3.AUX_ADC_IRQ 3Bh = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_ALMOST_FULL 3Ch = AUX_EVCTL:EVSTAT3.AUX_ADC_FIFO_NOT_EMPTY 3Dh = AUX_EVCTL:EVSTAT3.AUX_SMPH_AUTOTAKE_DONE 3Fh = No event. |
SWWUTRIG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_SWWUTRIG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_SWWUTRIG_TABLE.
Return to the Summary Table.
Software Wakeup Triggers
System CPU uses these wakeup flags to perform handshaking with AUX_SCE. The wakeup flags can change the operational mode of AUX and guarantees a non-zero SCE clock rate. AUX_SCE wakeup vectors are configured in VECCFGn.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | SW_WU3 | SW_WU2 | SW_WU1 | SW_WU0 | |||
| R-0h | W-0h | W-0h | W-0h | W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3 | SW_WU3 | W | 0h | Software wakeup 3 trigger. 0: No effect. 1: Set WUFLAGS.SW_WU3 and trigger AUX wakeup. |
| 2 | SW_WU2 | W | 0h | Software wakeup 2 trigger. 0: No effect. 1: Set WUFLAGS.SW_WU2 and trigger AUX wakeup. |
| 1 | SW_WU1 | W | 0h | Software wakeup 1 trigger. 0: No effect. 1: Set WUFLAGS.SW_WU1 and trigger AUX wakeup. |
| 0 | SW_WU0 | W | 0h | Software wakeup 0 trigger. 0: No effect. 1: Set WUFLAGS.SW_WU0 and trigger AUX wakeup. |
WUFLAGS is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUFLAGS_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUFLAGS_TABLE.
Return to the Summary Table.
Wakeup Flags
This register holds the eight AUX wakeup flags. Each flag can cause AUX operational mode to change as given in OPMODEREQ. To clear flag n you must set bit n in WUFLAGSCLR until flag n is read as 0. You must clear bit n in WUFLAGSCLR before flag n can be set again.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SW_WU3 | SW_WU2 | SW_WU1 | SW_WU0 | PROG_WU3 | PROG_WU2 | PROG_WU1 | PROG_WU0 |
| R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h | R-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | SW_WU3 | R | 0h | Software wakeup 3 flag. 0: Software wakeup 3 not triggered. 1: Software wakeup 3 triggered. |
| 6 | SW_WU2 | R | 0h | Software wakeup 2 flag. 0: Software wakeup 2 not triggered. 1: Software wakeup 2 triggered. |
| 5 | SW_WU1 | R | 0h | Software wakeup 1 flag. 0: Software wakeup 1 not triggered. 1: Software wakeup 1 triggered. |
| 4 | SW_WU0 | R | 0h | Software wakeup 0 flag. 0: Software wakeup 0 not triggered. 1: Software wakeup 0 triggered. |
| 3 | PROG_WU3 | R | 0h | Programmable wakeup 3. 0: Programmable wakeup 3 not triggered. 1: Programmable wakeup 3 triggered. |
| 2 | PROG_WU2 | R | 0h | Programmable wakeup 2. 0: Programmable wakeup 2 not triggered. 1: Programmable wakeup 2 triggered. |
| 1 | PROG_WU1 | R | 0h | Programmable wakeup 1. 0: Programmable wakeup 1 not triggered. 1: Programmable wakeup 1 triggered. |
| 0 | PROG_WU0 | R | 0h | Programmable wakeup 0. 0: Programmable wakeup 0 not triggered. 1: Programmable wakeup 0 triggered. |
WUFLAGSCLR is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUFLAGSCLR_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUFLAGSCLR_TABLE.
Return to the Summary Table.
Wakeup Flags Clear
This register clears AUX wakeup flags WUFLAGS.
To clear programmable wakeup flags you must disable the AUX wakeup output first. After the programmable wakeup flags are cleared you must re-enable the AUX wakeup output. Write WUGATE to disable or enable the AUX wakeup output. This procedure is not required when you want to clear a software-triggered wakeup.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SW_WU3 | SW_WU2 | SW_WU1 | SW_WU0 | PROG_WU3 | PROG_WU2 | PROG_WU1 | PROG_WU0 |
| R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-1h | R/W-1h | R/W-1h | R/W-1h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7 | SW_WU3 | R/W | 0h | Clear software wakeup flag 3. 0: No effect. 1: Clear WUFLAGS.SW_WU3. Keep high until WUFLAGS.SW_WU3 is 0. |
| 6 | SW_WU2 | R/W | 0h | Clear software wakeup flag 2. 0: No effect. 1: Clear WUFLAGS.SW_WU2. Keep high until WUFLAGS.SW_WU2 is 0. |
| 5 | SW_WU1 | R/W | 0h | Clear software wakeup flag 1. 0: No effect. 1: Clear WUFLAGS.SW_WU1. Keep high until WUFLAGS.SW_WU1 is 0. |
| 4 | SW_WU0 | R/W | 0h | Clear software wakeup flag 0. 0: No effect. 1: Clear WUFLAGS.SW_WU0. Keep high until WUFLAGS.SW_WU0 is 0. |
| 3 | PROG_WU3 | R/W | 1h | Programmable wakeup flag 3. 0: No effect. 1: Clear WUFLAGS.PROG_WU3. Keep high until WUFLAGS.PROG_WU3 is 0. The wakeup flag becomes edge sensitive if you write PROG_WU3 to 0 when PROGWU3CFG.EN is 1. The wakeup flag becomes level sensitive if you write PROG_WU3 to 0 when PROGWU3CFG.EN is 0, then set PROGWU3CFG.EN. |
| 2 | PROG_WU2 | R/W | 1h | Programmable wakeup flag 2. 0: No effect. 1: Clear WUFLAGS.PROG_WU2. Keep high until WUFLAGS.PROG_WU2 is 0. The wakeup flag becomes edge sensitive if you write PROG_WU2 to 0 when PROGWU2CFG.EN is 1. The wakeup flag becomes level sensitive if you write PROG_WU2 to 0 when PROGWU2CFG.EN is 0, then set PROGWU2CFG.EN. |
| 1 | PROG_WU1 | R/W | 1h | Programmable wakeup flag 1. 0: No effect. 1: Clear WUFLAGS.PROG_WU1. Keep high until WUFLAGS.PROG_WU1 is 0. The wakeup flag becomes edge sensitive if you write PROG_WU1 to 0 when PROGWU1CFG.EN is 1. The wakeup flag becomes level sensitive if you write PROG_WU1 to 0 when PROGWU1CFG.EN is 0, then set PROGWU1CFG.EN. |
| 0 | PROG_WU0 | R/W | 1h | Programmable wakeup flag 0. 0: No effect. 1: Clear WUFLAGS.PROG_WU0. Keep high until WUFLAGS.PROG_WU0 is 0. The wakeup flag becomes edge sensitive if you write PROG_WU0 to 0 when PROGWU0CFG.EN is 1. The wakeup flag becomes level sensitive if you write PROG_WU0 to 0 when PROGWU0CFG.EN is 0, then set PROGWU0CFG.EN. |
WUGATE is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUGATE_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_WUGATE_TABLE.
Return to the Summary Table.
Wakeup Gate
You must disable the AUX wakeup output:
- Before you clear a programmable wakeup flag.
- Before you change the value of [PROGWUnCFG.EN] or [PROGWUnCFG.WU_SRC].
The AUX wakeup output must be re-enabled after clear operation or programmable wakeup configuration.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | EN | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | EN | R/W | 0h | Wakeup output enable. 0: Disable AUX wakeup output. 1: Enable AUX wakeup output. |
VECCFG0 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG0_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG0_TABLE.
Return to the Summary Table.
Vector Configuration 0
AUX_SCE wakeup vector 0 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 0. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG1 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG1_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG1_TABLE.
Return to the Summary Table.
Vector Configuration 1
AUX_SCE wakeup vector 1 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 1. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG2 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG2_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG2_TABLE.
Return to the Summary Table.
Vector Configuration 2
AUX_SCE wakeup vector 2 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 2. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG3 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG3_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG3_TABLE.
Return to the Summary Table.
Vector Configuration 3
AUX_SCE wakeup vector 3 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 3. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG4 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG4_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG4_TABLE.
Return to the Summary Table.
Vector Configuration 4
AUX_SCE wakeup vector 4 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 4. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG5 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG5_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG5_TABLE.
Return to the Summary Table.
Vector Configuration 5
AUX_SCE wakeup vector 5 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 5. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG6 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG6_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG6_TABLE.
Return to the Summary Table.
Vector Configuration 6
AUX_SCE wakeup vector 6 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 6. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
VECCFG7 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG7_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_VECCFG7_TABLE.
Return to the Summary Table.
Vector Configuration 7
AUX_SCE wakeup vector 7 configuration
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | VEC_EV | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | VEC_EV | R/W | 0h | Select trigger event for vector 7. Non-enumerated values are treated as NONE. 0h = Vector is disabled. 1h = WUFLAGS.PROG_WU0 2h = WUFLAGS.PROG_WU1 3h = WUFLAGS.PROG_WU2 4h = WUFLAGS.PROG_WU3 5h = WUFLAGS.SW_WU0 6h = WUFLAGS.SW_WU1 7h = WUFLAGS.SW_WU2 8h = WUFLAGS.SW_WU3 9h = AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY |
EVSYNCRATE is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_EVSYNCRATE_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_EVSYNCRATE_TABLE.
Return to the Summary Table.
Event Synchronization Rate
Configure synchronization rate for certain events to the synchronous AUX event bus.
You must select SCE rate when AUX_SCE uses the event. You must select AUX bus rate when system CPU uses the event.
SCE rate equals rate configured in AON_PMCTL:AUXSCECLK. AUX bus rate equals SCE rate, or SCLK_HF divided by two when MCU domain is active.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | AUX_COMPA_SYNC_RATE | AUX_COMPB_SYNC_RATE | AUX_TIMER2_SYNC_RATE | ||||
| R-0h | R/W-0h | R/W-0h | R/W-0h | ||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-3 | RESERVED | R | 0h | Reserved |
| 2 | AUX_COMPA_SYNC_RATE | R/W | 0h | Select synchronization rate for AUX_EVCTL:EVSTAT2.AUX_COMPA event.
0h = SCE rate 1h = AUX bus rate |
| 1 | AUX_COMPB_SYNC_RATE | R/W | 0h | Select synchronization rate for AUX_EVCTL:EVSTAT2.AUX_COMPB event.
0h = SCE rate 1h = AUX bus rate |
| 0 | AUX_TIMER2_SYNC_RATE | R/W | 0h | Select synchronization rate for: - AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV0 - AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV1 - AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV2 - AUX_EVCTL:EVSTAT3.AUX_TIMER2_EV3 - AUX_EVCTL:EVSTAT3.AUX_TIMER2_PULSE 0h = SCE rate 1h = AUX bus rate |
PEROPRATE is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PEROPRATE_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_PEROPRATE_TABLE.
Return to the Summary Table.
Peripheral Operational Rate
Some AUX peripherals are operated at either SCE or at AUX bus rate.
You must select SCE rate when AUX_SCE uses such peripheral or an event produced by it. You must select AUX bus rate when system CPU uses such peripheral.
SCE rate equals rate configured in AON_PMCTL:AUXSCECLK. AUX bus rate equals SCE rate, or SCLK_HF divided by 2 when MCU domain is active.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ANAIF_DAC_OP_RATE | TIMER01_OP_RATE | SPIM_OP_RATE | MAC_OP_RATE | |||
| R-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3 | ANAIF_DAC_OP_RATE | R/W | 0h | Select operational rate for AUX_ANAIF DAC sample clock state machine.
0h = SCE rate 1h = AUX bus rate |
| 2 | TIMER01_OP_RATE | R/W | 0h | Select operational rate for AUX_TIMER01.
0h = SCE rate 1h = AUX bus rate |
| 1 | SPIM_OP_RATE | R/W | 0h | Select operational rate for AUX_SPIM.
0h = SCE rate 1h = AUX bus rate |
| 0 | MAC_OP_RATE | R/W | 0h | Select operational rate for AUX_MAC.
0h = SCE rate 1h = AUX bus rate |
ADCCLKCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_ADCCLKCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_ADCCLKCTL_TABLE.
Return to the Summary Table.
ADC Clock Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ACK | REQ | |||||||||||||
| R-0h | R-0h | R/W-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | ACK | R | 0h | Clock acknowledgement. 0: ADC clock is disabled. 1: ADC clock is enabled. |
| 0 | REQ | R/W | 0h | ADC clock request. 0: Disable ADC clock. 1: Enable ADC clock. Only modify REQ when equal to ACK. |
TDCCLKCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TDCCLKCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TDCCLKCTL_TABLE.
Return to the Summary Table.
TDC Counter Clock Control
Controls if the AUX_TDC counter clock source is enabled. TDC counter clock source is configured in DDI_0_OSC:CTL0.ACLK_TDC_SRC_SEL.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ACK | REQ | |||||||||||||
| R-0h | R-0h | R/W-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. |
| 1 | ACK | R | 0h | TDC counter clock acknowledgement. 0: TDC counter clock is disabled. 1: TDC counter clock is enabled. |
| 0 | REQ | R/W | 0h | TDC counter clock request. 0: Disable TDC counter clock. 1: Enable TDC counter clock. Only modify REQ when equal to ACK. |
TDCREFCLKCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TDCREFCLKCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TDCREFCLKCTL_TABLE.
Return to the Summary Table.
TDC Reference Clock Control
Controls if the AUX_TDC reference clock source is enabled. This clock is compared against the AUX_TDC counter clock. TDC reference clock source is configured in DDI_0_OSC:CTL0.ACLK_REF_SRC_SEL.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ACK | REQ | |||||||||||||
| R-0h | R-0h | R/W-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | ACK | R | 0h | TDC reference clock acknowledgement. 0: TDC reference clock is disabled. 1: TDC reference clock is enabled. |
| 0 | REQ | R/W | 0h | TDC reference clock request. 0: Disable TDC reference clock. 1: Enable TDC reference clock. Only modify REQ when equal to ACK. |
TIMER2CLKCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKCTL_TABLE.
Return to the Summary Table.
AUX_TIMER2 Clock Control
Access to AUX_TIMER2 is only possible when TIMER2CLKSTAT.STAT is different from NONE.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | SRC | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-3 | RESERVED | R | 0h | Reserved |
| 2-0 | SRC | R/W | 0h | Select clock source for AUX_TIMER2. Update is only accepted if SRC equals TIMER2CLKSTAT.STAT or TIMER2CLKSWITCH.RDY is 1. It is recommended to select NONE only when TIMER2BRIDGE.BUSY is 0. A non-enumerated value is ignored. 0h = no clock 1h = SCLK_LF 2h = SCLK_MF 4h = SCLK_HF / 2 |
TIMER2CLKSTAT is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKSTAT_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKSTAT_TABLE.
Return to the Summary Table.
AUX_TIMER2 Clock Status
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | STAT | ||||||||||||||
| R-0h | R-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-3 | RESERVED | R | 0h | Reserved |
| 2-0 | STAT | R | 0h | AUX_TIMER2 clock source status.
0h = No clock 1h = SCLK_LF 2h = SCLK_MF 4h = SCLK_HF / 2 |
TIMER2CLKSWITCH is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKSWITCH_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2CLKSWITCH_TABLE.
Return to the Summary Table.
AUX_TIMER2 Clock Switch
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RDY | ||||||||||||||
| R-0h | R-1h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | RDY | R | 1h | Status of clock switcher. 0: TIMER2CLKCTL.SRC is different from TIMER2CLKSTAT.STAT. 1: TIMER2CLKCTL.SRC equals TIMER2CLKSTAT.STAT. RDY connects to AUX_EVCTL:EVSTAT3.AUX_TIMER2_CLKSWITCH_RDY. |
TIMER2DBGCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2DBGCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2DBGCTL_TABLE.
Return to the Summary Table.
AUX_TIMER2 Debug Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | DBG_FREEZE_EN | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | DBG_FREEZE_EN | R/W | 0h | Debug freeze enable. 0: AUX_TIMER2 does not halt when the system CPU halts in debug mode. 1: Halt AUX_TIMER2 when the system CPU halts in debug mode. |
CLKSHIFTDET is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_CLKSHIFTDET_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_CLKSHIFTDET_TABLE.
Return to the Summary Table.
Clock Shift Detection
A transition in the MCU domain state causes a non-accumulative change to the SCE clock period when the AUX clock rate is derived from SCLK_MF or SCLK_LF:
- A single SCE clock cycle is 6 thru 8 SCLK_HF cycles longer when MCU domain enters active state.
- A single SCE clock cycle is 6 thru 8 SCLK_HF cycles shorter when MCU domain exits active state.
AUX_SCE detects if such events occurred to the SCE clock during the time period between a clear of STAT and a read of STAT.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | STAT | ||||||
| R-0h | R/W-1h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | STAT | R/W | 1h | Clock shift detection. Write: 0: Restart clock shift detection. 1: Do not use. Read: 0: MCU domain did not enter or exit active state since you wrote 0 to STAT. 1: MCU domain entered or exited active state since you wrote 0 to STAT. |
RECHARGETRIG is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RECHARGETRIG_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RECHARGETRIG_TABLE.
Return to the Summary Table.
VDDR Recharge Trigger
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TRIG | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | TRIG | R/W | 0h | Recharge trigger. 0: No effect. 1: Request VDDR recharge. Request VDDR recharge only when AUX_EVCTL:EVSTAT2.PWR_DWN is 1. Follow this sequence when OPMODEREQ.REQ is LP: - Set TRIG. - Wait until AUX_EVCTL:EVSTAT2.VDDR_RECHARGE is 1. - Clear TRIG. - Wait until AUX_EVCTL:EVSTAT2.VDDR_RECHARGE is 0. Follow this sequence when OPMODEREQ.REQ is PDA or PDLP: - Set TRIG. - Clear TRIG. |
RECHARGEDET is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RECHARGEDET_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RECHARGEDET_TABLE.
Return to the Summary Table.
VDDR Recharge Detection
Some applications can be sensitive to power noise caused by recharge of VDDR. You can detect if VDDR recharge occurs.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | STAT | EN | |||||
| R-0h | R-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | STAT | R | 0h | VDDR recharge detector status. 0: No recharge of VDDR has occurred since EN was set. 1: Recharge of VDDR has occurred since EN was set. |
| 0 | EN | R/W | 0h | VDDR recharge detector enable. 0: Disable recharge detection. STAT becomes zero. 1: Enable recharge detection. |
RTCSUBSECINC0 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINC0_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINC0_TABLE.
Return to the Summary Table.
Real Time Counter Sub Second Increment 0
INC15_0 will replace bits 15:0 in AON_RTC:SUBSECINC when RTCSUBSECINCCTL.UPD_REQ is set.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | INC15_0 | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | INC15_0 | R/W | 0h | New value for bits 15:0 in AON_RTC:SUBSECINC. |
RTCSUBSECINC1 is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINC1_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINC1_TABLE.
Return to the Summary Table.
Real Time Counter Sub Second Increment 1
INC23_16 will replace bits 23:16 in AON_RTC:SUBSECINC when RTCSUBSECINCCTL.UPD_REQ is set.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | INC23_16 | ||||||||||||||||||||||||||||||
| R-0h | R/W-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-8 | RESERVED | R | 0h | Reserved |
| 7-0 | INC23_16 | R/W | 0h | New value for bits 23:16 in AON_RTC:SUBSECINC. |
RTCSUBSECINCCTL is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINCCTL_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSECINCCTL_TABLE.
Return to the Summary Table.
Real Time Counter Sub Second Increment Control
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | UPD_ACK | UPD_REQ | |||||
| R-0h | R-0h | R/W-0h | |||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-2 | RESERVED | R | 0h | Reserved |
| 1 | UPD_ACK | R | 0h | Update acknowledgement. 0: AON_RTC has not acknowledged UPD_REQ. 1: AON_RTC has acknowledged UPD_REQ. |
| 0 | UPD_REQ | R/W | 0h | Request AON_RTC to update AON_RTC:SUBSECINC. 0: Clear request to update. 1: Set request to update. Only change UPD_REQ when it equals UPD_ACK. Clear UPD_REQ after UPD_ACK is 1. |
RTCSEC is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSEC_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSEC_TABLE.
Return to the Summary Table.
Real Time Counter Second
System CPU must not access this register. Instead, system CPU must access AON_RTC:SEC.VALUE directly.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | SEC | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | SEC | R | 0h | Bits 15:0 in AON_RTC:SEC.VALUE. Follow this procedure to get the correct value: - Do two dummy reads of SEC. - Then read SEC until two consecutive reads are equal. |
RTCSUBSEC is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSEC_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCSUBSEC_TABLE.
Return to the Summary Table.
Real Time Counter Sub-Second
System CPU must not access this register. Instead, system CPU must access AON_RTC:SUBSEC.VALUE directly.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | SUBSEC | ||||||||||||||||||||||||||||||
| R-0h | R-0h | ||||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-0 | SUBSEC | R | 0h | Bits 31:16 in AON_RTC:SUBSEC.VALUE. Follow this procedure to get the correct value: - Do two dummy reads SUBSEC. - Then read SUBSEC until two consecutive reads are equal. |
RTCEVCLR is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCEVCLR_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_RTCEVCLR_TABLE.
Return to the Summary Table.
AON_RTC Event Clear
Request to clear events:
- AON_RTC:EVFLAGS.CH2.
- AON_RTC:EVFLAGS.CH2 delayed version.
- AUX_EVCTL:EVSTAT2.AON_RTC_CH2.
- AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | RTC_CH2_EV_CLR | ||||||
| R-0h | R/W-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | RTC_CH2_EV_CLR | R/W | 0h | Clear events from AON_RTC channel 2. 0: No effect. 1: Clear events from AON_RTC channel 2. Keep RTC_CH2_EV_CLR high until AUX_EVCTL:EVSTAT2.AON_RTC_CH2 and AUX_EVCTL:EVSTAT2.AON_RTC_CH2_DLY are 0. |
BATMONBAT is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_BATMONBAT_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_BATMONBAT_TABLE.
Return to the Summary Table.
AON_BATMON Battery Voltage Value
Read access to AON_BATMON:BAT. System CPU must not access this register. Instead, system CPU must access AON_BATMON:BAT directly. AON_BATMON:BAT updates during VDDR recharge or active operational mode.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 | 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | INT | FRAC | |||||||||||||||||||||||||||||
| R-0h | RH-0h | R-0h | |||||||||||||||||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-11 | RESERVED | R | 0h | Reserved |
| 10-8 | INT | RH | 0h | See AON_BATMON:BAT.INT. Follow this procedure to get the correct value: - Do two dummy reads of INT. - Then read INT until two consecutive reads are equal. |
| 7-0 | FRAC | R | 0h | See AON_BATMON:BAT.FRAC. Follow this procedure to get the correct value: - Do two dummy reads of FRAC. - Then read FRAC until two consecutive reads are equal. |
BATMONTEMP is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_BATMONTEMP_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_BATMONTEMP_TABLE.
Return to the Summary Table.
AON_BATMON Temperature Value
Read access to AON_BATMON:TEMP. System CPU must not access this register. Instead, system CPU must access AON_BATMON:TEMP directly. AON_BATMON:TEMP updates during VDDR recharge or active operational mode.
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SIGN | INT | FRAC | |||||||||||||
| R-0h | RH-0h | R-0h | |||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-16 | RESERVED | R | 0h | Reserved |
| 15-11 | SIGN | R | 0h | Sign extension of INT. Follow this procedure to get the correct value: - Do two dummy reads of SIGN. - Then read SIGN until two consecutive reads are equal. |
| 10-2 | INT | RH | 0h | See AON_BATMON:TEMP.INT. Follow this procedure to get the correct value: - Do two dummy reads of INT. - Then read INT until two consecutive reads are equal. |
| 1-0 | FRAC | R | 0h | See AON_BATMON:TEMP.FRAC. Follow this procedure to get the correct value: - Do two dummy reads of FRAC. - Then read FRAC until two consecutive reads are equal. |
TIMERHALT is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMERHALT_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMERHALT_TABLE.
Return to the Summary Table.
Timer Halt
Debug register
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | PROGDLY | AUX_TIMER2 | AUX_TIMER1 | AUX_TIMER0 | |||
| R-0h | RH/W-0h | RH/W-0h | RH/W-0h | RH/W-0h | |||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3 | PROGDLY | RH/W | 0h | Halt programmable delay. 0: AUX_EVCTL:PROGDLY.VALUE decrements as normal. 1: Halt AUX_EVCTL:PROGDLY.VALUE decrementation. |
| 2 | AUX_TIMER2 | RH/W | 0h | Halt AUX_TIMER2. 0: AUX_TIMER2 operates as normal. 1: Halt AUX_TIMER2 operation. |
| 1 | AUX_TIMER1 | RH/W | 0h | Halt AUX_TIMER01 Timer 1. 0: AUX_TIMER01 Timer 1 operates as normal. 1: Halt AUX_TIMER01 Timer 1 operation. |
| 0 | AUX_TIMER0 | RH/W | 0h | Halt AUX_TIMER01 Timer 0. 0: AUX_TIMER01 Timer 0 operates as normal. 1: Halt AUX_TIMER01 Timer 0 operation. |
TIMER2BRIDGE is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2BRIDGE_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_TIMER2BRIDGE_TABLE.
Return to the Summary Table.
AUX_TIMER2 Bridge
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | BUSY | ||||||
| R-0h | R-0h | ||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-1 | RESERVED | R | 0h | Reserved |
| 0 | BUSY | R | 0h | Status of bus transactions to AUX_TIMER2. 0: No unfinished bus transactions. 1: A bus transaction is ongoing. |
SWPWRPROF is shown in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_SWPWRPROF_FIGURE and described in #AUX_SYSIF_AUX_SYSIF_MMAP_AUX_SYSIF_AUX_SYSIF_ALL_SWPWRPROF_TABLE.
Return to the Summary Table.
Software Power Profiler
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | STAT | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-3 | RESERVED | R | 0h | Reserved |
| 2-0 | STAT | R/W | 0h | Software status bits that can be read by the power profiler. |