SLUS987C January 2011 – December 2019
PRODUCTION DATA.
When the capacitor array has been fully charged (indicated by OperationStatus[FC] being set) then it is monitored for excessive leakage.
When Current exceeds CLBAD Current the [CLBAD] flag in SafetyAlert is set.
When Current exceeds CLBAD for a period greater than CLBAD Time the [CLBAD] flag in SafetyStatus is set.
This function is disabled if CLBAD Time is set to 0.
In a weak capacitor condition, charging is disabled and the CHG FET is turned off, ChargingCurrent and ChargingVoltage() are set to 0.
The weak capacitor fault is cleared when Current falls equal to or below the CLBAD Recovery limit. When the recovery condition is detected, then the CHG FET is allowed to be turned on, if other safety and configuration states permit, ChargingCurrent and ChargingVoltage() are set to the appropriate value per the charging algorithm, and the [CLBAD] flag in SafetyStatus is reset.