SLUS987C January 2011 – December 2019
PRODUCTION DATA.
The BQ33100 periodically determines the capacitance and equivalent series resistance (ESR) of the super capacitor array during normal operation. The Learning Frequency is a register that sets the time between automatic learning cycles of the super capacitor, which can also be manually executed by issuing a Learn command. The BQ33100 uses the learning cycles to update the Capacitance and ESR registers accordingly, and both are accessible through the SMBus interface.
The learning process is a multi-step procedure fully controlled by the BQ33100 that will perform the following sequence to learn capacitance and ESR:
where:
and