SLUS987C January 2011 – December 2019
PRODUCTION DATA.
This read-word function returns an unsigned integer value of the temperature in units of 0.1°K, as measured by the BQ33100. It has a range of 0 to 6553.5°K. The source of the measured temperature is configured by the [TEMP1] and [TEMP0] bits in the Operation Cfg register.
SBS CMD | MODE | NAME | FORMAT | SIZE IN BYTES | MIN VALUE | MAX VALUE | DEFAULT VALUE | UNIT |
---|---|---|---|---|---|---|---|---|
0x08 | R | Temperature | Unsigned Integer | 2 | 0 | 65535 | — | 0.1°K |