SLUS987C January 2011 – December 2019
PRODUCTION DATA.
This read- or write-block command allows the user to change the Unseal key for the Sealed-to-Unsealed security-state transition. This function is only available when the BQ33100 is in the UNSEALED mode, indicated by a cleared [SS] flag.
The order of the bytes, when entered in ManufacturerAccess, is the reverse of what is written to or read from the part. For example, if the 1st and 2nd word of the UnSealKey block read returns 0x1234 and 0x5678, then in ManufacturerAccess, 0x3412 and 0x7856 must be entered to unseal the part.
SBS CMD | MODE | NAME | FORMAT | SIZE IN BYTES | MIN VALUE | MAX VALUE | DEFAULT VALUE | UNIT |
---|---|---|---|---|---|---|---|---|
0x60 | R/W | UnSealKey | Hex | 4 | 0x00000000 | 0xffffffff | — |