SLUS987C January 2011 – December 2019
PRODUCTION DATA.
During the operation lifetime of the BQ33100, it gathers voltage data . During this time, the BQ33100 can be enabled to record the maximum value that the measured voltage reached. If the [LTE] flag is set, Lifetime Max Capacitor Voltage is updated if one of the following conditions are met:
SUBCLASS ID | SUBCLASS NAME | OFFSET | NAME | FORMAT | SIZE IN BYTES | MIN VALUE | MAX VALUE | DEFAULT VALUE | UNIT |
---|---|---|---|---|---|---|---|---|---|
59 | Lifetime Data | 4 | Lifetime Max Capacitor Voltage | Integer | 2 | 0 | 32767 | 0 | mV |