SLUS987C January 2011 – December 2019
PRODUCTION DATA.
Instructs the BQ33100 to enable access to the SBS functions and data flash space and clear the [SS] flag. This two-step command needs to be written to ManufacturerAccess in the following order: 1st word of the UnSealKey followed by the 2nd word of the UnSealKey. If the command fails 4 seconds must pass before the command can be reissued. This command is only available when the BQ33100 is in SEALED mode. See Security (Enables and Disables Features) for detailed information.