SLUS987C January 2011 – December 2019
PRODUCTION DATA.
The BQ33100 determines charge termination if:
NOTE
To make sure that the charge terminates properly, TI recommends that Taper Current be set to a value greater than the maximum charger voltage inaccuracy. In other words, the charger taper current must be set to a lower value than the taper current programmed in the dataflash to ensure proper charge termination and the FC bit gets set.
The BQ33100 sets the [FC] flag in OperationStatus() when a valid charge termination occurs and cleared when RelativeStateOfCharge is less than FC Clear %.
The taper voltage must be set to a value less than the OV threshold. This prevents an over voltage condition from occuring after the CL bit clears upon learning completion.
The BQ33100 can also determine charge termination if the RSOC is at a value equal to or greater than FC set %. If this is not the desired means of charge termination, FC set % must be set to -1%.