SLUS987C January 2011 – December 2019
PRODUCTION DATA.
The BQ33100 can receive data with or without PEC. In the write-word protocol, the BQ33100 receives the PEC after the last byte of data from the host. If the host does not support PEC, the last byte of data is followed by a stop condition. After receipt of the PEC, the BQ33100 compares the value to its calculation. If the PEC is correct, the BQ33100 responds with an ACKNOWLEDGE. If it is not correct, the BQ33100 responds with a NOT ACKNOWLEDGE.