SLUS987C January 2011 – December 2019
PRODUCTION DATA.
This read-word function returns a signed integer value of the measured current being supplied (or accepted) by the super capacitor pack in mA, with a range of –32768 to 32767. A positive value indicates charge current and a negative value indicates discharge.
Any current value within the Deadband will be reported as 0 mA by the Current function.
SBS CMD | MODE | NAME | FORMAT | SIZE IN BYTES | MIN VALUE | MAX VALUE | DEFAULT VALUE | UNIT |
---|---|---|---|---|---|---|---|---|
0x0A | R | Current | Unsigned Integer | 2 | –32768 | 32767 | — | mA |