SLUS987C January 2011 – December 2019
PRODUCTION DATA.
During the normal operation of the BQ33100 the CHG output of the BQ33100 is typically controlled automatically but can be overridden through the CHGOR pin (pin 21). On a low-to-high transition the CHG output is released turning off the external CHG FET and on a high-to-low transition the CHG output is pulled low after a programmable delay CHG Enable Delay. If CHG Enable Delay is programmed to 0 the delay is a maximum of 250 ms. If the CHG override function is not needed, then the CHGOR pin must connect to VSS.