SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Each TR which is processed, provides the ability to assert 1 of 4 possible output events at specific completion levels for the TR. Since the output event is specified directly in the TR and the TRs are written by potentially untrusted software processes, channels are only able to assert virtual events when they complete various portions of the TR. These virtual events are then mapped to actual destination events in the global event map by the TCHAN UDMA_TOES_j or RCHAN UDMA_ROES_j event steering registers. These registers are programmed statically by a trusted software process that has determined the channels that should have access to the specified event destination slots.