SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The CSI_RX_IF stream interface provides the usual VSYNC/HSYNC signals. The signals are per virtual channel where the transition from 1-to-0 or 0-to-1 represents SOF/EOF or SOL/EOL. VSYNC/HSYNC transition is usually not coincident with a valid data phase, though there are use cases where it can be. Because of the nature of CSI protocol, the VSYNC and HSYNC transactions require at least a single clock cycle and can only transition sequentially (important fact in handling of VSYNC events).
There is a rarely used mode of CSI where an entire frame is passed in a single packets without line breaks. In this mode, there are no HSYNC transitions at line starts/ends.
Lastly, there is redundant information provided with each CSI packet where the packet length is supplied in bytes.
To overcome these framing restrictions, the CSI_RX_IF PSILSS0 passes metadata through the DMA FIFO. Anytime metadata is inserted into the FIFO, the CSI_RX_IF stream is stalled for a clock cycle. The forms of supported meta tags are:
The PSILSS0 will disregard the HSYNC signal entirely. The long packet beginning is used as SOL and the EOL will be "counted" using the packet length provided. In the special case where packets are of FRAME length, the SOL/EOL handling is identical.
The PSILSS0 solution for VSYNC handling is to create the concept of metadata FIFO entry which is indicated by a metadata bit. The SOF or EOF VSYNC information plus the virtualChan index is fed into the FIFO. On the output of the FIFO, the SOF is saved for each context of that virtualChan type. The very next data phase of that channel context will be marked as SOF. Additionally a state bit per context is maintained indicating the channel is MOP (middle of packet). Once the EOF arrives at the FIFO output, all contexts of that type virtual channel (and currently in MOP state) will receive a PSI_EOP with zero active bytes of data.
The line and frame size is not known outside the CSI core (i.e. not passed to the DMA interface). Therefore any mismatches at system level programming will be unknown. If the DMA line/frame size does not match the CSI_RX_IF line/frame size, it is assumed the DMA will not result in any adverse side affects as a result of not enough data or too much data.