SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The R5FSS has several slave interfaces that define its internal memory space:
Regions [0] and [1] of the TCM slave interface provide direct access to the TCM RAMs. Access to the RAMs is arbitrated with access from the R5F’s L1 memory system. Excessive access while the R5F is also attempting access will degrade performance.
Regions [2] and [3] of the TCM slave interface provide access to the cache RAMs for testing purposes. Access to the cache RAMs can only be done while the caches are disabled and should only be done for test purposes.
In addition to the slave interfaces, there are peripherals (RAT and VIM) that are only accessible by the R5F. The R5F has an access to these modules via the VBUSP peripheral interface.