SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
A Command Timeout happens when a command is presented on the destination side but never accepted within the allotted time. See Command Timeout Error Reporting. When this happens, a Command Timeout interrupt is issued. When servicing a Command Timeout Error, software should perform the following step:
When a Command Timeout occurs. The gasket automatically transitions to Software Flush mode (see Flush Mode). The system can assume that the target infrastructure is hung and take appropriate action. Suggested actions include: