SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
RINGACC provides an overflow function where a push to a full ring will result in a push to a special overflow ring, rather than just losing the pushed data. The overflow ring is defined through the RINGACC_OVRFLOW register, and that ring must be defined with a large enough element size to cover the element size of any other ring, as well as enough elements to hold enough overflow data (as an overflow to the overflow ring will be lost). When there is a push to a full ring, there will be two elements written to the overflow ring, first the push data, and then the ring number that was full. A supervisor entity can own the overflow ring and perform what actions are needed from the overflow data. The size of the overflow ring must be an even number since two elements will be pushed for each overflow event. The overflow ring must be configured in ring or message modes.