SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The standard Message ID (11-bit ID) filtering flow is shown in Figure 12-326. Section 12.4.4.3.10.5, Standard Message ID Filter Element describes the standard Message ID filter element.
The Remote Transmission Request (RTR) and Extended Identifier (XTD) bits of the received frames are compared against the list of configured filter elements. This is controlled by the following registers:
Figure 12-326 Standard Message ID Filter Path