SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Ethernet port 1
The total number of frames received on the port that experienced an alignment error or code error. Such a frame:
Overruns have no effect upon this statistic.
An alignment error is defined to be:
A code error is defined to be a frame which has been discarded because the port’s MRXER pin driven with a one for at least one bit-time’s duration at any point during the frame’s reception.
RFC 1757 etherStatsCRCAlignErrors Ref. 1.5 can be calculated by summing Rx Align/Code Errors and Rx CRC errors.