SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The Power-AP has a DEBUGENABLE directive that is used to drive a "debug active" signal to the associated cores in the managed domain. When the tools set this directive, the debug logic in a CPU or other debugable module is automatically activated. This is particularly valuable when the subdomain is completely powered down, but there is a desire for debug capability (breakpoints) immediately after it is repowered.