SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The trace aggregator has a 32-bit input bus interface for collecting data from various trace sources. The arbitration scheme is such that trace sources behave in a cooperative manner to ensure that their data is received within the timing boundaries allocated for any HLTM. It is required that:
Note that the trace aggregator has no HW protection to prevent trace sources form violating these rules. If one or more trace sources attached to the aggregator violates these rules, the data from all sources may be corrupt.