SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
Once mesh block fetch is completed, final input co-ordinates are calculated by applying back mapping on previously calculated perspective warp corner pixel co-ordinates. Additional padding is applied on top of these back mapped corner co-ordinates based on the interpolation type.
The LDC processes a block of VPAC_LDC_OUT_BLKSZ[7:0] OBW x VPAC_LDC_OUT_BLKSZ[15:8] OBH (output block width by output block height) pixels at a time in a raster-scan order throughout the image. OBW is constrained to be a multiple of a base width, depending on the operating mode. This is described in Table 6-158. OBH should be even. The LDC uses four corners of the output block plus some padding to fetch the input block. Due to extreme scenarios, there will be scenarios where above bounding box calculated by hardware doesn’t cover all the input data required to generate particular output block. To cover those cases, software needs to supply additional PixelPad, the amount of padding in input block in all directions. Software must supply OBW, OBH, and VPAC_LDC_OUT_BLKSZ[19:16] PIXPAD, the amount of padding in input pixels. Software must guarantee that, for EVERY output pixel in the OBW x OBH output block, the input pixels required are bounded by back mapping of the four corners plus/minus the padding. More precisely, the input block is determined by:
where corner1, corner2, corner3, and corner4 are upper-left, upper-right, lower-left, and lower-right corners of the OBW x OBH output block, and distortx(.), distorty(.) are X and Y distorted coordinates of the corners. Distorted coordinates computed by the back-mapping process described in Section 6.7.4.2.7, LDC Lens Distortion Back-Mapping. Figure 6-130 shows the input block bound calculation. Table 6-158 lists the OBW requirements.
Figure 6-130 LDC Input Block Bound| Data Format | OBW must be a multiple of |
|---|---|
| YUV422 | 8 |
| YUV420 | 8 |
Typically for geometric distortion, the LDC_BLOCK[19:16] PIXPAD bit field must be 4 to accommodate neighbor sets for all colors. Software must set the PIXPAD bit field correctly.
OBH and OBW must be large enough for efficient operation of the lens distortion operation. As shown in Table 6-158, OBW is constrained to ensure efficient external memory write. Another constraint is that input block size, (IBX_end – IBX_start + 1) x (IBY_end - IBY_start + 1), for EVERY input block of the image, must fit the allocated input buffer. These parameters must not be specified pessimistically (OBH, OBW too small, or PixelPad too large). Pessimistic parameter setting degrades performance and incurs unnecessary external memory transfer.
The LDC can process a portion of the image, rather than the entire image. This saves time by letting an image process through multiple software/LDC interactions to correct only a portion of the image (See Multi-pass Frame processing).
An intermediate event, hts_tdone, is also provided on completion of each macro block output write. This allows the LDC operation to be pipelined with other tasks. The LDC output write stall after this event, waiting for a pulse on the hts_tstart signal to begin writing the next macro block.