The ECC aggregator has ECC control, status and interrupt registers for each ECC endpoint in a module or subsystem. These registers are memory mapped and occupy 1 KB address space although part of it may contain reserved locations. The registers are split in the following types:
- Global registers. They are common to all
ECC endpoints associated with the ECC aggregator and include the ECC_VECTOR
and ECC_REV registers. Each ECC endpoint has assigned a unique ID. When this
ID is written to the ECC_VECTOR[10-0] ECC_VECTOR field the corresponding
endpoint is selected either for control or for status reading.
- ECC control and status registers. These
registers are specific to each ECC endpoint and reside in the range from
address offset 0x10 to 0x28, if the endpoint is ECC RAM or from 0x10 to
0x24, if the endpoint is interconnect ECC component. They are memory mapped
but are accessed through the ECC serial interface. They are also selected by
the ECC endpoint ID written to the ECC_VECTOR[10-0] ECC_VECTOR field.
Because of latency on the serial interface the ECC control and status
registers are read by performing special sequence as described in Section 12.10.6.2.3. These registers have also different functionality for both types of
endpoints - ECC RAM and interconnect ECC component.
- Interrupt registers. They include
interrupt status, interrupt enable, interrupt disable, and EOI registers.
For more information, see Interrupts.