SPRUJ52E June 2022 – September 2025 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4APE-Q1 , TDA4VH-Q1 , TDA4VP-Q1 , TDA4VPE-Q1
The tear down completion process is when software has set the DRU_CHRT_CTL_j[30] TEARDOWN bit to 0x1 so no new TRs can be added to the channel but when previous TRs that had been added to the channel are still running. Once the TR FIFO for the channel is empty hardware clears the DRU_CHRT_CTL_j[30] TEARDOWN and DRU_CHRT_CTL_j[31] ENABLE bits. The channel is now back at the channel configuration process as described in Section 10.4.3.1.2.1 and can be reused as needed by the system.