Geometric distortions, barrel and pincushion distortion, can be corrected on UYVY and NV12 data formats. The Mesh based back mapping is used in this mode. An additional affine transform can be configured at the same time.
- Check and wait for VPAC_LDC_CTRL[2] BUSY to
become IDLE (0).
- Set VPAC_LDC_CTRL[4-3] IP_DATAMODE for UYVY (0)
or NV12 data (2). Program VPAC_LDC_CTRL[6-5]
IP_DFMT to required data storage format.
- Set VPAC_LDC_CTRL[1] LDMAPEN = 1 to enable lens
distortion back mapping.
- Set the input frame base address in
VPAC_LDC_RD_BASE_H / VPAC_LDC_RD_BASE_L registers.
Note that the frame base address must be aligned
on a 16-byte boundary. In case of YUV420,
YUV422SP, Y1_Y2 and Y1_Y2Y3 modes, configure
VPAC_LDC_RD_420C_BASE_H / VPAC_LDC_RD_420C_BASE_L
registers for Chroma Data.
- Set the input frame line offset in
VPAC_LDC_RD_OFST[15-0] OFST.
- If reading the input image from a circular buffer:
- Set VPAC_LDC_CTRL[9] IP_CIRCEN = 1.
- LDC computes the row number and applies modulo
operation. The absolute address in the buffer is
computed from this wrap-around row and the column
number and then data is fetched from the circular
buffer. Set the circular buffer size in
VPAC_LDC_RD_OFST[29-16] MOD register field. In
YUV420 modes, the number of rows in the buffer is
MOD/2. In others modes, the number of rows in the
buffer is MOD for both Y buffer and Cb/Cr
buffer.
- Set the tile size in
VPAC_LDC_REGION_OUT_BLKSZ_j[15-8] OBH and
VPAC_LDC_REGION_OUT_BLKSZ_j[7:0] OBW. Note the
constraints on OBW in Table 6-158.
- Set the pixel pad in
VPAC_LDC_REGION_OUT_BLKSZ_j[19-16] PIXPAD.
- Set the input frame size in
VPAC_LDC_INPUT_FRSZ[29-16] H and
VPAC_LDC_INPUT_FRSZ[13-0] W.
- Set the output frame size in
VPAC_LDC_MESH_FRSZ[29-16] H and
VPAC_LDC_MESH_FRSZ[13:0] W. Mesh data has to be
present for entire frame after transform.
- Set the output compute frame size in
VPAC_LDC_COMPUTE_FRSZ[29-16] H and
VPAC_LDC_COMPUTE_FRSZ[13-0] W.
- Set the starting output point in
VPAC_LDC_INITXY[12-0] INITX and
VPAC_LDC_INITXY[28-16] INITY.
- Configure SL2 Interface programming registers. Details of LSE configuration is captured in Section 6.7.4.3.4.
- Set the mesh offset table pointer to the correct
address (VPAC_LDC_MESH_BASE_H /
VPAC_LDC_MESH_BASE_I[31-0] ADDR and
VPAC_LDC_MESH_OFST[15-0] OFST). Set the table down
sampling factor for MxM down sampling in
VPAC_LDC_MESHTABLE_CFG[2-0] M.
- Set the Y plane interpolation type to bilinear or
bi-cubic in VPAC_LDC_CFG[6] YINT_TYP.
- If also using affine transform, set the six
affine transform parameters in VPAC_LDC_AFF_AB.A,
VPAC_LDC_AFF_AB.B, VPAC_LDC_AFF_CD.C,
VPAC_LDC_AFF_CD.D, VPAC_LDC_AFF_EF.E, and
VPAC_LDC_AFF_EF.F. If affine transform is not
used, then these need to be set to the following
values: A = 4096, B = 0, C = 0, D = 0, E = 4096,
and F = 0.
- If also using perspective transform, enable
VPAC_LDC_CTRL[7] PWARPEN and set
VPAC_LDC_PWARP_GH[15-0] G and
VPAC_LDC_PWARP_GH[31-16] H. If perspective
transform is not used, disable VPAC_LDC_CTRL[7]
PWARPEN and set VPAC_LDC_PWARP_GH[15-0] G = 0 and
VPAC_LDC_PWARP_GH[31-16] H = 0.
- Set VPAC_LDC_CTRL[0] LDC_EN = 1 to start the LDC
operation.
- Start the HTS init sequencing. LDC fetch/processing is gated with hts_init.
- Wait for VPAC_LDC_CTRL[2] BUSY to become IDLE (0)
or wait for the end of frame completion
interrupt.