SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The timer can be configured to provide a programmable PWM output. The timer PWM (POTIMERPWM) output pin can be configured to toggle on an event. The DMTIMER1MS_TCLR[11-10] TRG bit field determines on which register value the PWM pin toggles. Either overflow or both overflow and match can be selected to toggle the timer PWM pin when a compare condition occurs.
In toggle mode, when DMTIMER1MS_TCLR[11-10] TRG = 0x2 (overflow and match), the first event that toggles the PWM line is an overflow event.
The DMTIMER1MS_TCLR[7] SCPWM bit can be programmed to set or clear the timer PWM output signal only while the counter is stopped or the trigger is off. This allows setting the output pin to a known state before modulation starts. Modulation synchronously stops when the DMTIMER1MS_TCLR[11-10] TRG bit field is cleared and overflow occurs. This allows fixing a deterministic state of the output pin when modulation stops.
In Figure 12-453, the internal overflow pulse is set each time the (0xFFFF FFFF – DMTIMER1MS_TLDR[31-0] LOAD_VALUE + 1) value is reached, and the internal match pulse is set when the counter reaches the value of DMTIMER1MS_TMAR. Depending on the value of the DMTIMER1MS_TCLR[12] PT bit and DMTIMER1MS_TCLR[11-10] TRG bit field, the timer provides pulse or PWM event on the output pin (POTIMERPWM).
The DMTIMER1MS_TLDR and DMTIMER1MS_TMAR must keep values below the overflow value (0xFFFF FFFF) by at least two units. If the PWM trigger events are both overflow and match, the difference between the values kept in the DMTIMER1MS_TMAR and the value in the DMTIMER1MS_TLDR must be at least two units. When match event is used, the compare mode DMTIMER1MS_TCLR[6] CE bit must be set.
In Figure 12-453, the DMTIMER1MS_TCLR[7] SCPWM bit is set to 0. In Figure 12-454, the DMTIMER1MS_TCLR[7] SCPWM bit is set to 1. To obtain the desired wave form, start the counter at 0xFFFF FFFE value (to ensure an overflow first) or adjust the line polarity (DMTIMER1MS_TCLR[7] SCPWM bit).
Figure 12-453 Timing
Diagram of PWM With DMTIMER1MS_TCLR[7] SCPWM Bit = 0
Figure 12-454 Timing
Diagram of PWM With DMTIMER1MS_TCLR[7] SCPWM Bit = 1