SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Descriptor starvation occurs when the Port receives enough data for a burst but the ring for the channel is currently empty. This causes push back on the receive port and can cause lost data.
The Port will assert a starvation bit in the RX Receive Channel Status register (RCHANRT[a]_RRT_STATUS[1-0]). When the doorbell register (RINGRT[a]_RT_DB) is written to populate the ring the starvation bit will clear. Note that the intention is that the port will wait for an entry to be added to the ring. It is assumed that if data loss is not desired that the host will guarantee that a descriptor is present.