SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
| Bits | Field | Reset | Description |
|---|---|---|---|
| 31 | enable | 0x0 | When set, the channel is enabled. When cleared, the RX channel is disabled. When disabled, the channel ignores all DMA events from the peripheral. It maintains proper data transfers with the UDMA-P such that the credit handshake is not disrupted. However, unlike teardown, it does not close out the current open packet. Thus the teardown bit should always be used to disable an RX channel instead of manually clearing this bit. Failing to use teardown may result in stale data remaining in the internal RX FIFO, which would also prevent the channel from going idle without a channel reset. Note that this bit cannot be changed from 0 to 1 if the global enable bit in the peer enable register is 0. |
| 30 | tdown | 0x0 | When set, the channel will commence a RX channel teardown procedure. It will stop on the next FIFO boundary. It then clears the DMA event count and ignores all future DMA events from the peripheral. After stopping peripheral reads, the PDMA sends a teardown message to the UDMA-P that also closes the current packet with an EOP. If no packet is open at the time of the teardown, the message also includes SOP. The EOP teardown message may or may not contain final packet data. Once the channel teardown is complete and ready to be reused, the enable bit is cleared. |
| 29 | pause | 0x0 | When set, the channel is in a paused state. It will stop on the next FIFO boundary. It continues to accept and count DMA events from the peripherals, but will not act on them. The pause bit can be cleared and data will resume. Pause will not stop teardown from completing. |
| 28:2 | - | 0x0 | Reserved. |
| 1 | idle | 0x0 | This is a read-only bit that signifies that the Paused or Disabled channel is also idle. This bit is read only and can only become set if pause is set or enable is cleared. |
| 0 | free | 0x0 | Free Run: 0 = channel honors the emudbg suspend signal, 1 = channel will free run, regardless of the value of emudbg suspend. |