SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Figure 12-235 Auto CMD12 Error RecoveryThe sequence for Auto CMD12 Error Recovery is shown in Figure 12-235. Following four cases A-D shall be covered.
A: An error occurred in CMD_wo_DAT, but not in the SD memory transfer.
B: An error occurred in CMD_wo_DAT, and also occurred in the SD memory transfer.
C: An error did not occur in CMD_wo_DAT, but an error occurred in the SD memory transfer.
D: CMD_wo_DAT was not issued, and an error occurred in the SD memory transfer.
(1) Check MMCSD0_AUTOCMD_ERR_STS[0] ACMD12_NOT_EXEC bit. If this bit is set to 1, go to step (2). If this bit is set to 0, go to step (6). In addition, the Host Driver shall define PCMD flag, which changes to 1 if MMCSD0_AUTOCMD_ERR_STS[0] ACMD12_NOT_EXEC bit is set to 1.
(2) Wait for Error Interrupt Recovery for CMD_wo_DAT.
(3) Check "Return Status". In the case of "Non-recoverable Error", go to step (16). In the case of "Recoverable Error", go to step (4).
(4) Issue CMD12 .
(5) If the CMD line errors occur for the CMD12 (one of D03-00 is set in the MMCSD0_ERROR_INTR_STS register), "Return Status" is "Non-recoverable Error" and go to step (16). If not CMD line error and busy timeout error occur (D04 is set in the MMCSD0_ERROR_INTR_STS register), "Return Status" is "Recoverable Error" and go to step (11). Otherwise, "Return Status" is "No error" and go to step (17).
(6) Set MMCSD0_SOFTWARE_RESET[1] SWRST_FOR_CMD bit to 1 for software reset of the CMD line.
(7) Check MMCSD0_SOFTWARE_RESET[1] SWRST_FOR_CMD bit. If MMCSD0_SOFTWARE_RESET[1] SWRST_FOR_CMD bit is 0, go to step (8). If it is 1, go to step (7).
(8) Issue CMD12 . Acceptance of CMD12 depends on the state of the card. CMD12 may make the card to return to tran state. If the card is already in tran state, the card does not response to CMD12.
(9) Check "Return Status" for CMD12. If "Return Status" returns "Non-recoverable Error", go to step (16). In the case of "Recoverable Error" or "No error", go to step (10).
(10) Check the MMCSD0_AUTOCMD_ERR_STS[0] ACMD12_NOT_EXEC bit. If this bit is 0, go to step (11). If it is 1, go to step (14).
(11) Set MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit to 1 for software reset of the DAT line.
(12) Check MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit. If MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit is 0, go to step (13). If it is 1, go to step (12).
(13) Check the PCMD flag. If PCMD is 1, go to step (18). If it is 0, go to step (19).
(14) Set MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit to 1 for software reset of the DAT line.
(15) Check MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit. If MMCSD0_SOFTWARE_RESET[2] SWRST_FOR_DAT bit is 0, go to step (20). If it is 1, go to step (15).
(16) Return Status of "Non-recoverable Error".
(17) Return Status that an error has occurred in CMD_wo_DAT, but not in the SD memory transfer.
(18) Return Status that an error has occurred in both CMD_wo_DAT, and the SD memory transfer.
(19) Return Status that an error has not occurred in CMD_wo_DAT, but has occurred in the SD memory transfer.
(20) Return Status that CMD_wo_DAT has not been issued, and an error has occurred in the SD memory transfer.