SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Each proxy thread can produce events based on the state of the resource it uses. For outbound proxy threads, a threshold can be set so that an event is produced when there are now at least N messages available to write. For inbound proxy threads, a threshold can be set so that an event is produced when there are now at least N messages available to read. These threshold values are programmed in SEC_PROXY_EVT_MAP_j, allowing the host to determine how often it gets events. Programming the count values while the threshold is set to 0 will not trigger events, but if the threshold is not 0 then programming the counts will trigger events based on whether the threshold is reached or not. No event is generated if the event is programmed to 0xFFFF.