The following features are not
supported on this family of devices:
- The following apply to 4-bit
MMCSD instances:
- SD Card busy LED: Not
pinned out
- The following apply to 8-bit
MMCSD instances:
- SD Card busy LED -
Not pinned out
- SD/SDIO/MMC Cards
(Removable) - no support for 4-pin/8-pin muxing
- SD Card Detect Pin -
Not pinned out
- SD Card Write Protect
Pin - Not pinned out
- Enhanced Strobe
- IO retention
- Muxing of LVCMOS functions with the PHY at the SoC level