The MDIO module includes a user access register
(MDIO CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k, where k = 0 or 1) to directly access
a specified PHY device. To read a PHY register, perform the following:
- Check to ensure that the GO bit in the MDIO user
access register (CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k, where k = 0 or 1) is
cleared.
- Write to the GO, REGADR, and PHYADR bits in the
CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register corresponding to the PHY and
PHY register SW wants to read.
- The read data value is available in the DATA bit
field in MDIO CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register after the module
completes the read operation on the serial bus. Completion of the read operation
can be determined by polling the GO and ACK bits in
CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k register. After the GO bit has cleared,
the ACK bit is set on a successful read.
- Completion of the operation sets the
corresponding USERINTRAW bit (0 or 1) in the MDIO user command complete
interrupt register (CPSW3_MDIO_USER_INT_RAW_REG) corresponding to MDIO
CPSW3_MDIO_USER_GROUP_USER_ACCESS_REG_k used. If interrupts have been enabled on
this bit using the MDIO user command complete interrupt mask set register
(CPSW3_MDIO_USER_INT_MASK_SET_REG), then the bit is also set in the MDIO user
command complete interrupt register (CPSW3_MDIO_USER_INT_MASKED_REG) and an
interrupt is triggered on the host processor.