SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The CSI_TX_IF may be configured to perform a combination of the scenarios outlined in the previous sections if sufficient streams are available. One or more streams may be ganged with Stream0 to perform data type interleaving on the same virtual channel, whilst the remaining streams may be left autonomous to perform virtual channel interleaving.
In this case, the same rules governing the use of the virtual channels and data types must be observed. In this scenario, the virtual channel signals will be configured to the single value required for the ganged group (as they need to be controlled within the same frame valid active signal) and different values for those left to be autonomous (as they may generate their own frame start and frame end events).The slave stream for each virtual channel can have a different data type selected, and this may change on a line-by-line (or packet-by-packet) basis.