SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
A watermark monitor tracks the low and high values of the data source since the last read of the monitor. After initial setup or clearing, the watermark values will load the current value of the data source as the low and high. Then for successive operations if the resulting data source of the queue is below the low watermark, or above the high watermark, the associated watermark will be updated. When the monitor value registers are read, the value is cleared and starts tracking again using the current data source value. This can be useful for tracking low and high values of queue element counts or sizes for data tracking, debug or future optimizations, such as allocating items to a queue or buffer sizes based on counts.