SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
An overlay manager (OVR) is responsible for composting selected input layers together to generate the final display output frame. DISPC implements two identical overlay managers (see DISPC Architecture Overview):
Each OVR is preceded by a programmable input pipeline selector which re-maps the outputs of the selected input pipeline according to the overlay manager z-order configuration.
The output of each OVR is connected to the Color Phase Rotation (CPR) unit through a gamma table of the corresponding video port.
Figure 12-545 DISPC Overlay Manager and
Input SelectorThe DISPC overlay managers, OVR1 and OVR2, will be commonly referred to as overlay manager (OVR) in the following sections.