SPRUJB3C March 2024 – November 2025 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
| Bits | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | valid | r/o | 0 |
Indicates that the num field of this register is valid. This field is set whenever the IRQ Vector Address (Base Address + 0x18) is read. It is cleared whenever the IRQ Vector Address (Base Address + 0x18) is written. 1 – num field is valid (active IRQ interrupt) 0 – num field is invalid (no active IRQ interrupts) |
| 30:20 | reserved | r/o | 0 | Always read as 0. Writes have no effect. |
| 19:16 | pri | r/o | 0 | This field indicates the priority of the active IRQ interrupt. This field is only valid if the valid flag (bit 31) is set. Otherwise the value is unpredictable |
| 15:10 | reserved | r/o | 0 | Always read as 0. Writes have no effect. |
| 9:0 | num | r/o | 0 |
This field indicates the interrupt number of the active IRQ interrupt. This field is loaded with the value from the Prioritized IRQ (Base Address + 0x08) whenever the IRQ Vector Address (Base Address + 0x18) is read. This field is only valid if the valid flag (bit 8) is set. Otherwise the value is unpredictable 0 – Interrupt 0 1 – Interrupt 1 1023 – Interrupt 1023 Note: The highest value is determined by the num_groups parameter |