SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The CSI_RX_IF will detect the error condition and capture the associated VC, DT and WC information for the packet header before generating an error interrupt flag on CSIRX_ERROR_IRQS.
The CSI_RX_IF will continue processing the current frame and continue the stream when a header Reserved DT or a long packet payload CRC error is detected.
The CSI_RX_IF will stop processing the current frame and continue the stream when a packet header ECC error is detected, as the current frame synchronisation cannot be maintained.