SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
After reset, all threads on PSI-L are uninitialized and unpaired. The Host will pair each source PDMA channel with (typically) a corresponding destination channel in the UDMA-P. The PDMA thread is configured to point to the UDMA-P thread and the UDMA-P thread is configured to point to the PDMA thread. Once paired, the source channels in the PDMA will send all their data to the source channel in the UDMA-P and the destination channel in the UDMA-P will never see any data other than data from the source channel in the PDMA.