SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The direct command mechanism is a way to send commands (with a maximum size of direct_cmd_fifodepth bytes) by writing and reading registers. It allows commands to be sent that are not allowed through the SDI-DSI interface (DSI commands, triggers), to perform read operations or to send DCS / generic write / generic read operations when the DSI link is not fully programmed and cannot use the SDI interface for commands.
Figure 12-529 shows direct command management sequence.
Basically, the procedure to do so is as follows:
The command should be started only if the command request is amongst the defined ones for DCS or Generic Write or Read with 0, 1, or more parameters:
Note: The direct_cmd_main_settings register can use other data type values for cmd_head to support future types and no check is performed for invalid types.
There are several checks performed when sending a direct command to verify that requested command sizes are supported and to check that the requested command exists (otherwise the request to send the command is ignored).
At completion of a read command, registers can be read (they contain read data and/or errors detected during the communication) and trigger events are sent to the application to announce the request completion (using the status and error register bank).
When a read request is performed, the read data is put in the RP FIFO. If more bytes are sent, they are ignored and errors are set accordingly. The received read can then be accessed by reading several times the register that gives an access to the FIFO.
For every new command, several status bits are present: one signals that a command is being transmitted (cmd_transmission). When the command is complete, several bits can be toggled to signal it (write_completed, trigger_completed, te_received, read_completed and read_completed_with_err).
Some complex commands provide intermediate information. For BTA requests, there is a bit that signals when the BTA request has been sent (BTA_completed) and another one that signals when the DSI is controller of the D-PHY interface again (BTA_finished). For commands that imply a BTA, some other bits specify whether specific data has been received (such as trigger, acknowledge with or without error).