SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
In the SPI boot mode, the ROM Code initializes the OSPI peripheral to SPI mode and the image is read from the flash memory connected to the corresponding OSPI port and chip-select. A detailed summary of the SPI boot parameter table and the boot configuration definitions are listed in Section 5.6.3, OSPI/QSPI/SPI Boot Parameter Table. If the image fails to be read correctly from offset 0x0 of the flash memory, the ROM will attempt to obtain the image at offset 0x400000. This is the only redundant image location supported by the ROM.