SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
An unsupported feature error is returned for a TR that is received that cannot be run because it specifies a feature that is optional and not supported by the BCDMA that received the TR. The STATUS INFO specifies the feature that was not supported. If it specifies multiple features that were not supported the BCDMA implementation can determine which type it wants to return.
Value | Submission Error Type |
---|---|
0 | TR Type not supported |
1 | STATIC not supported |
2 | EOL not supported |
3 | CONFIGURATION SPECIFIC not supported |
4 | AMODE not supported |
5 | ELTYPE not supported |
6 | DFMT not supported |
7 | SECTR not supported |
8 | AMODE SPECIFIC Field not supported |
9-15 | Reserved |