SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
This section shows an example on how to utilize RAT block to allow R5 to access 36 SoC Memory Map. The RAT block inside R5 has up to 8 address remapping regions.
Assuming R5 needs to access the following region:
First of all, we need to construct 32b R5 memory map as following and how those memory spaces are mapped to SoC level, shown in Table 7-33. Users can define where the OSPI and DDR data space placed inside R5’s memory map and how they should be mapped to SoC level address map. Table 7-33 just shows one of the many possible ways to construct the memory map.
R5 Memory Map(32b) | SoC Memory Map (36b) | RAT Remapping | |
---|---|---|---|
SoC Level peripheral and on-chip SRAM (This is guaranteed by SoC Hardware design. No user configuration is needed) |
0x0 to 0x7FFF_FFFF Same address as SoC memory map |
0x0 to 0x7FFF_FFFF | Not RAT Remapping |
512MB OSPI data region (user defined) |
0x8000_0000 to 0x9FFF_FFFF | 0x4_0000_0000 to 0x4_1FFF_FFFF | Using RAT remapping region 0 |
512MB DDR space (user defined) |
0xA000_0000 to 0xBFFF_FFFF | 0x8000_0000 to 0x9FFF_FFFF | Using RAT remapping region 1 |
Additional 1GB DDR Space (user defined) |
0xC000_0000 to 0xFFFF_FFFF | 0x9_0000_0000 to 0x9_3FFF_FFFF | Using RAT remapping region 2 |
In this example, only three RAT regions are needed:
In order achieving those mappings, those are the setting of the RAT configuration registers:
Region 0 | Region 1 | Region 2 | Other regions | |
---|---|---|---|---|
Region control register | Enabled, size set to 512MB | Enabled, size set to 512MB | Enabled, size set to 1GB | disabled |
Region base(32b) | 0x8000_0000 | 0xA000_0000 | 0xc000_0000 | Don’t care |
Region translated lower address(32b) | 0x0000_0000 | 0x8000_0000 | 0x0000_0000 | Don’t care |
Region translated upper address | 0x4 | 0x0 | 0x9 | Don’t care |
Figure 7-18 shows how RAT is remapping the address between R5’s 32b address to 36b SoC address.