SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
For Rx channels which are not configured in single buffer mode, if the host provides a buffer chain whose total length is insufficient to receive the entire packet, whatever portion of the packet which has not been received will be flushed until an end of packet indicator is received on the PSI-L interface. This behavior will occur regardless of which error handling mode has been selected for the channel.