SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Software must keep the CSI_TX_IF_CONTROL1[0] PIXEL_RESET register in the asserted state in the control register until all CSI_TX_IF controller registers are programmed. Only after all CSI_TX_IF controller programming can software de-assert CSI_TX_IF_CONTROL1 register. If software has to reprogram any CSI_TX_IF controller registers it MUST have the control CSI_TX_IF_CONTROL1 register reset asserted.
It is a restriction that LS/LE detection is disabled.