SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The CSI_TX_IF can support interleaving of virtual channels by using two or more pixel interfaces and configuring the value of the virtual channels signal differently on each interface. The data streams can then be controlled using the pixel_dt_sel_if inputs to select the data type for the lines. In this scenario, each pixel interface must have exclusive use of the virtual channel. Each stream will generate its own frame start and frame end synchronisation packets. In this case, all the stream protocol modules employing virtual channel interleaving must be configured as masters by clearing the STREAM_IF_*_SLAVE_MODE bit in the STREAM_IF_*_CFG registers.
Note that the virtual channel control input is sampled at the rising edge of the frame_valid_if input, and thereafter remains fixed for that frame, therefore the virtual channel cannot be switched on a line-by-line basis for any single pixel interface. While it is possible to switch the Virtual Channel control input from frame to frame, the timing-critical switching required here would indicate a requirement for hardware rather than software control.