SPRUJB6B November 2024 – May 2025 AM2612
The MMC/SD/SDIO host controller uses a data buffer. This buffer transfers data from one data bus (Interconnect) to another data bus (SD, SDIO, or MMC card bus) and vice versa.
The buffer is the heart of the interface and ensures the transfer between the two interfaces (L4 and the card). To enhance performance, the data buffer is completed by a prefetch register and a post-write buffer that are not accessible by the host controller.
The read access time of the prefetch register is faster than the one of the data buffer. The prefetch register allows data to be read from the data buffer at an increased speed by preloading data into the prefetch register.
The entry point of the data buffer, the prefetch buffer, and the post-write buffer is the 32-bit register MMC_DATA. A write access to the MMC_DATA register followed by a read access from the MMC_DATA register corresponds to a write access to the post-write buffer followed by a read access to the prefetch buffer. As a consequence, it is normal that the data of the write access to the MMC_DATA register and the data of the read access to the MMC_DATA register are different.
The number of 32-bit accesses to the MMC_DATA register that are needed to read (or write) a data block with a size of MMC_BLK[10:0] BLEN, and equals the rounded up result of BLEN divided by 4. The maximum block size supported by the host controller is hard-coded in the register MMC_CAPA[17:16] MBL field and cannot be changed.
A read access to the MMC_DATA register is allowed only when the buffer read enable status is set to 1 (MMC_PSTATE[11] BRE); otherwise, a bad access (MMC_STAT[29] BADA) is signaled.
A write access to the MMC_DATA register is allowed only when the buffer write enable status is set to 1 (MMC_PSTATE[10] BWE); otherwise, a bad access (MMC_STAT[29] BADA) is signaled and the data is not written.
The data buffer has two modes of operation to store and read of the first and second portions of the data buffer:
The MMC_CMD[4] DDIR bit must be configured before a transfer to indicate the direction of the transfer.
Figure 13-191 shows the buffer management for writing and Figure 13-192 shows the buffer management for reading.
Figure 13-191 Buffer Management for a Write
Figure 13-192 Buffer Management for a Read