SPRUJB6B November 2024 – May 2025 AM2612 , AM2612-Q1
Underflow occurs when an operation generates a value that is too small to represent in the given floating-point format. Under such cases, a zero value is returned. If a TMU operation generates an underflow condition, then the latched underflow flag (LUF) is set to 1. The LUF flag will remain latched until cleared by the user executing an instruction that clears the flag. It also generates an interrupt to the respective R5 Core R5FSS*_CORE*_INTR_R5SS0_CPU0_TMU_LUF(#210)