SPRUJB6B November 2024 – May 2025 AM2612
In emulation mode, the SCIGCR1.CONT bit determines how the LIN operates when the program is suspended. The LIN counters are affected by this bit during debug mode. When this bit is set, the counters are running even when a debug halt occurs. When cleared, the counters stop counting when a debug halt occurs.
Any reads in emulation mode to a LIN register do not have any effect on the flags in the SCIFLR register.